Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an EZM315125, Series M01 branch unit?

Issue:
Repair parts

Product Line:
EZM Metering

Resolution:
Only the parts listed below are considered field replaceable:

Customer Cover ,(includes labels) - EZM315125C (Obsolete)
Cover Screws - 4020513002K (Includes 10 screws per kit)
Meter Socket Cover (cover for one-meter position) - MMC
Meter Socket Sealing Ring (aluminum latch type) - 2920910001
Parts Kit (one position, meter socket line side through tenant breaker base) - MM125KIT
Circuit Breaker RB Cover (one position) - BCV
Enclosure connecting hardware and Service Disconnect labels - 7329791750
Mounting Channel - 7329772301 (Obsolete)
Equipment Ground Bar Assembly:
(1) 73298-970-54 (bracket with 5 lugs mounted to it)
(2) 2142217101 (mounting screws for the ground bar assembly)
End Closing Cap Kit - EZMCAP
End Closing Cap Kit (Right Side Only Shallow) - EZMSCAP
Top Endwall Rain Cap – 7329714601
Top Endwall Rain Cap Mounting Screws – 4020513002K (Includes 10 screws; only 2 screws are used to secure the rain cap)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings