Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MP86200, Series M01 branch unit?
Issue:
Current Design repair parts

Product Line:
Meter Pak Metering

Resolution:
Only the parts listed below are considered field replaceable:
Customer Covers (includes labels) - (2) MP6200C
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Meter Socket Cover (ring type, one position) - MMC
Meter Socket Sealing Ring (aluminum latch type) - 2920910001
Pull Box Cover - MP56200PC
Line Phase and Neutral Lugs - MMLK500
Alternate Lug Kits - Refer to Digest
LEFT Meter Sockets Load Neutral and Service Ground Lug Assembly - 7329704351 (assembly includes 5 lugs and bus bar the lugs are mounted on)
RIGHT Meter Sockets Load Neutral and Service Ground Lug Assembly - 7329704353 (assembly includes 3 lugs and bus bar the lugs are mounted on)
Mounting Screws for BOTH Load Neutral/Service Ground Assembly:
(1) 2142720163 (mounts the right side of the LEFT assembly to the main neutral bar of the device)
(3) 2142717120 (1 screw is used to mount the left side of the LEFT assembly to the enclosure and 2 screws are used to mount the RIGHT assembly, one to the enclosure and one to the main neutral bar)

Equipment Ground Lug Assembly - 7329704451 (2 required, one for each set of meter sockets; each assembly includes 3 lugs and mounting bracket)
Mounting screws for EACH Equipment Ground Lug assembly - 2142217101 (2 per assembly)
Parts Kit (one position, meter socket line side through tenant breaker base) - MP200KIT
Mounting Channel - 7329652101

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings