Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can the BLANK meter socket/tenant breaker positions in a EZ METER-PAK branch unit be fitted with a meter socket and tenant circuit breaker in the field?

Issue:
Install an additional meter socket and a tenant circuit breaker in the field for the BLANK meter socket/tenant breaker position in the EZ Meter-pak branch unit.

Product Line:
Metering Equipment.

Environment:
EZ Metering Devices.

Resolution:
No. None of the following EZ METER-PAK branch units supplied with a BLANK position may be converted to include an additional meter socket and tenant circuit breaker position.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings