Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MPH33125, Series M01 branch unit?
Issue:
Current design repair parts

Product line:
Meter Pak Metering

Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover (includes labels) - MP3125C
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Blank Meter Socket Cover (top position) - MMCBK
Meter Socket Cover (ringless type, one position) - MMRC
Pull Box Cover - MP34125PC
Line Phase and Neutral Lugs - MMLK250
Load Neutral and Service Ground Lugs Assembly - 7329819855 (includes 5 lugs and bus bar the lugs are mounted on)
Mounting Screws for Load Neutral and Service Ground Assembly:
(1) 2142720163 - mounts the top of the assembly to the main neutral bar
(1) 2149020120 -  mounts the assembly to the enclosure, just below the main neutral connection
(1) 2153217161 - mounts the assembly at the bottom to the bracket attached to the enclosure

Equipment Ground Lugs Assembly - 7329897052 (includes 3 lugs and mounting bracket)
Mounting Screws for Equipment Ground Lug assembly - 2142217101 (2 required)
Parts Kit (one position, meter socket line side through tenant breaker base, does not include horn bypass kit, see below) - MM125KIT
Horn Type Bypass Kit - MMHB
Mounting Channel - 7329652001

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings