Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MPH44125, Series M01 branch unit?
Issue:
current design repair parts

Product Line:
Meter Pak Metering

Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover (includes labels) - MP4125C
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Meter Socket Cover (ringless type, one position) - MMRC
Pull Box Cover - MP34125PC
Line Phase and Neutral Lugs - MMLK250
Alternate Lug Kits - Refer to Digest
Load Neutral and Service Ground Lugs Assembly  - 7329819856 (includes 6 lugs and the bus bar the lugs are mounted on)
Mounting Screws for Load Neutral and Service Ground assembly:
(1) - 2142720163 (mounts the top of the assembly to the Main Neutral bus bar)
(1) - 2149020120 (mounts the middle of the assembly to the enclosure, just below the top mounting screw)
(1) - 2153217161 (mounts the bottom of the assembly to the bracket in the enclosure)

Equipment Ground Lugs Assembly  - 7329897053 (includes 4 lugs and the mounting bracket)
Mounting Screws for Equipment Ground Lug Assembly - (2) 2142217101
Parts Kit (one position, meter socket line side through tenant breaker base, does not include horn bypass kit, see below) - MM125KIT
Horn Type Bypass Kit - MMHB
Mounting Channel - 7329652001

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings