Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MPR55125, Series M01 branch unit?
Issue:
Current design repair parts

Product Line:
Meter Pak Metering

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover, Left Side (includes labels) - MP5125LC
Customer Cover, Right Side (includes labels) - MP5125RC
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Blank Meter Socket Cover (top left position) - MMCBK
Meter Socket Cover (ringless type, one position) - MMRC
Pull Box Cover - MP56125PC
Line Phase and Neutral Lugs - MMLK250
Alternate Lug Kits - Refer to Digest
Load Neutral and Service Ground Lugs Assembly: 7329819857 (includes connector and 4 lugs; used on the LEFT side of the pull box)
Load Neutral and Service Ground Lugs Assembly: 7329819862 (includes connector and 5 lugs; used on the RIGHT side of the pull box)
Mounting Screws: 2153217161, 2142720240 and 2149020120 (1 of each required per assembly)
Equipment Ground Lugs Assembly: 7329897051 (includes L-Bracket and 2 lugs; used on the LEFT side of the pull box)
Equipment Ground Lugs Assembly: 7329897052 (includes L-Bracket and 3 lugs; used on the RIGHT side of the pull box)
Mounting Screws: (4) 2142217101 (2 required per assembly)
Meter Socket Parts Kit (one position, meter socket line side through tenant breaker base) - MM125KIT
Mounting Channel - 7329652101

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings