Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a D222NRB, Series F01 general duty safety switch?
Issue:
Repair Parts

Product Line:
GD SS

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4056642150
Load base assembly - 4056002650
Base assembly mounting screw - 4020516001 (3 required for line base and 2 required for load base)
Arc shield - 4056001801
Arc shield mounting screw - 4020514501
Mechanism assembly - 4056637850
Handle assembly - 4056638750
Handle gasket - 4056608601
Lockplate - 4056638801
Lockplate mounting screw - 2299940562 (2 required)
Lug assembly - 4025101652
Neutral assembly - SN03
Neutral assembly mounting screw - 4020506501
Neutral bonding assembly - 4028365650
Cover latch and spring - 4056607201 and 4022304301

Schneider Electric USA

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings