Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H361RB, series F1?
Issue:
Repair Parts

Product Line:
HD SS

Resolution:
The repair parts for the H361RB, series F1(F01) are as follows. No other parts are available.
Line Base Assembly -4056642050 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 4056002550K (requires one per switch)
Arc Suppressor Assembly - 4056669451 (requires one per switch)
Lug Assembly - 4025101652 (per lug)
Switch Mechanism - 4056610750
Handle Assembly - 4056684150K
Handle Gasket - 4056603101
Lockplate - 4056637601

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings