Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an MPH64200, Series M01 branch unit?
Issue:
Current Design repair parts

Product Line:
Meter Pak Metering

Resolution:
Only the parts listed below are considered field replaceable:
Customer Cover (includes labels) - MP4200C
Circuit Breaker RB Cover (one position) - BCV
Cover Screws - 4020513002K
Meter Socket Cover (ringless type, one position) - MMRC
Pull Box Cover - MP4200PC
Line Phase and Neutral Lugs - MMLK250
Alternate Lug Kits - Refer to Digest
Load Neutral and Service Ground Lugs Assembly: 7329704350 (includes connector and six lugs)
Mounting Screws: (1) 21427-20163 and (1) 2142717120
Equipment Ground Lugs Assembly: 7329704450 (includes mounting bracket and four lugs)
Mounting Screws: (2) 2142217101
Parts Kit - MP200KIT (one position, meter socket line side through tenant breaker base; horn bypass kit not included)
Horn Type Bypass Kit - MMHB
Mounting Channel - 7329652001

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings