Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a D323NRB, series F01, F02, or F03 general duty safety switch?
Issue:
What are the replacement parts for a D323NRB Series F01, F02, or F03?

Product Line:
Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
  • Line base assembly - 4056603650
  • Load base assembly - 4056602850
  • Arc shield - 4056601901
  • Mechanism assembly - 4056647650
  • Handle assembly - 4056610350
  • Handle gasket - 4056608601
  • Lockplate - 4056605801
  • Lug assembly - 4025101851
  • Neutral assembly - SN0610
  • Base assembly mounting screws - 4020515101 (3 required for line base and 2 required for load base)
  • Arc shield mounting screw - 4020514501
  • Neutral bonding screw assembly - 4028365650
  • lockplate mounting screw - 2299940562 (2 required)
  • Lug assembly mounting screw - 4020514202

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings