Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU364RB, series F5? (may be shown as F05)

Article available in these languages: Spanish

Issue:
The list of repair parts is needed for Safety Switch catalog number HU364RB, series F5.

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the HU364RB, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base (all one part) - 4056703950 - (1 required; includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line/Load Base mounting screws - 4020546401 (6 required per line base)
Arc Suppressor Assembly - 4056677550 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - 4025116251 (per lug)
Lug Assembly mounting screw - 2140122240
Switch Mechanism - 4056678650 (also requires interlock shaft gasket 4056786001)
Switch Mechanism mounting screws- 2299940562 (2 required)
Handle Assembly - 4056663550 (also requires handle gasket 4056603101)
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings