Issue:
The list of repair parts is needed for Safety Switch catalog number HU364AWK, series F5.
Product Line:
Heavy Duty Safety Switch
Resolution:
The repair parts for the HU364AWK, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base (all one piece) - 4056704050 (1 required per switch; includes phynolic base, arc suppressors, lugs, rotor, and switching blades)
Line/Load Base mounting screws - 4020546401 (6 required per line base)
Arc Suppressor Assembly - 4056677550 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - CL20F (includes 6 lugs; requires mounting screws below)
Lug Assembly mounting screw - 2140122240 (per lug)
Switch Mechanism - 4056678650 (also requires interlock shaft gasket 4056786001)
Switch Mechanism mounting screws - 2299940562 (2 required)
Handle Assembly - 4056663550 (requires handle gasket 4056603101)
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Released for: Schneider Electric USA