Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the mounting screw torque, conductor size, and wire binding screw torque for PDC6MA20?
Issue:
What is the mounting screw torque, conductor size and wire binding screw torque for PDC6MA20?

Product Line:
Molded Case Circuit Breaker

Resolution:
- Mounting screw torque: 180 lb-in.
- Wire binding screw wrench size: 7/32 inch hex.
-Conductor quantity and sizes: 6 maximum
#3-#2/0 AWG Cu at 50 lb-in.
#6-#4 AWG Cu at 45 lb-in.
#8 AWG Cu at 40 lb-in.
#12-#10 AWG Cu at 35 lb-in.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings