Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What type of fuses are used with the L111N and L211N light duty safety switches?
Issue:
Design features

Product Line:
Light Duty Safety Switches

Resolution:
These switches accept the "Edison Base" plug type fuses. The switches are UL listed for use on systems with up to 10 kA RMS available fault current.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings