Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Where can the HLO1 handle clamp be used?

Issue:
On which breakers can the HLO1 handle clamp be used?

Product Line:
Miniature Circuit Breaker

Environment:
QO and Homeline Circuit Breakers

Resolution:
For 1, 2, or 3p QO or Q1 breakers, including CAFI, EPD, and GFI breakers, the HLO1 handle clamp can hold the handle in the ON or OFF position.

Note: The clamp will not fit over the LED handle of the new AF/AFGF breakers. The only option for AF/AFGF breakers is the padlock attachment QOADV1PAF.

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings