Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the D224N, series F1? (may be shown as F01)
Issue:
Design repair parts

Product Line:
General Duty Safety Switches

Resolution:
The replacement parts for the D224N, series F1 (F01) are as follows. No other parts are available.
Complete Line Base -4056702950 (1 required; includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
Line Base mounting screws - 4020546401 (6 required per line base)
Load Base Assembly - 4056677450 (1 required per phase; includes phenolic base, lugs, and fuse clips)
Load Base mounting screws - 4020546401 (2 required per load base)
Arc Suppressor Assembly - 4053922001 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - 4025116251 (per lug)
Lug Assembly mounting screw - 2140122240
Switch Mechanism - 4056678450
Switch Mechanism mounting screws - 2299940562 (2 required)
Handle Assembly - 4056686250
Lockplate - 4056685701
Lockplate mounting screws - 2299940562 (2 required)
Neutral Assembly - SN20A
Neutral Bonding Screw - 4028356651
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings