Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the DU324, series F1? (may be shown as F01)
Issue:
List of replaceable parts in DU324 series F1 general duty safety switch

Product line:
Safety switches

Resolution:
The replacement parts for the DU324, series F1 (F01) are as follows. No other parts are available.
  • Complete Line/Load Base - 4056703150 (1 required; includes phynolic base, arc suppressors, lugs, rotor, and switching blades)
  • Complete Line/Load Base mounting screws - 4020546401 (6 required per base)
  • Arc Suppressor Assembly - 4053922001 (1 required per phase)
  • Arc Suppressor mounting screw - 4020514501
  • Lug Assembly - 4025116251 (per lug)
  • Lug Assembly mounting screw - 2140122240
  • Switch Mechanism - 4056678450
  • Switch Mechanism mounting screws - 2299940562 (2 required)
  • Handle Assembly - 4056686250
  • Lockplate - 4056685701
  • Lockplate mounting screws - 2299940562 (2 required)
  • Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings