Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H324N, series F5? (may be shown as F05)

Issue:
The list of repair parts is needed for Safety Switch catalog number H324N, series F5.

Product Line:
Heavy Duty Safety Switch

Resolution:
The replacement parts for the H324N, series F5 (F05) are as follows. No other parts (enclosure, labels) are available.
Complete Line Base - 4056703050 - (1 required line base per switch - includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line Base mounting screws - 4020546401 (6 required per line base)
Load Base Assembly - 4056677450 (1 required per phase - includes phenolic base, lugs, and fuse clips)
Load Base mounting screws - 4020546401 (2 required per load base)
Arc Suppressor Assembly - 4053922001 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - 4025116251 (per lug)
Lug Assembly mounting screw - 2140122240
Switch Mechanism - 4056678650
Switch Mechanism mounting screws- 2299940562 (2 required)
Handle Assembly - 4056663550
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Neutral Assembly - SN20A
Neutral Bonding Screw - 4028356651
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings