Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H364NAWK, series F5? (may be shown as F05)
Product Line:
Heavy Duty Safety Switch H364NAWK, Series F5

Resolution:
The repair parts for the H364NAWK, series F5 (F05) are as follows. No other parts are available.
Complete Line Base - 4056703550 (1 required; includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
Line Base mounting screws - 4020546401 (6 required per line base)
Load Base Assembly - 4056678250 (1 required per phase; includes phenolic base, lugs, and fuse clips)
Load Base mounting screws - 4020546401 (2 required per load base)
Arc Suppressor Assembly - 4056677550 (1 required per phase)
Arc Suppressor mounting screw - 4020514501
Lug Assembly - CL20F (includes 6 lugs; requires mounting screws)
Lug Assembly mounting screw - 2140122240 (per lug)
Switch Mechanism - 4056678650 (also requires interlock shaft gasket 40567-860-01)
Switch Mechanism mounting screws- 2299940562 (2 required)
Handle Assembly - 4056663550 (requires handle gasket 40566-031-01)
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Neutral Assembly - SN20C
Neutral Bonding Screw - 4028356651

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings