Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H362N, series F5? (may be shown as F05)
Issue:
Repair parts

Product Line:
HD Safety Switch

Resolution:
The replacement parts for the H362N, series F5 (F05) are as follows:
Interior kit - HSIF3606F (includes line and load base assemblies, mechanism, arc suppressor, all mounting hardware, and instructions)
Load Base kit - HLB3606F (includes load base and mounting hardware)
Arc Suppressor kit - HAS0610F(includes arc suppressor and mounting hardware)
Lug kit - AL0306F (includes 6 lugs)
Handle/Mechanism kit- HM0610F (includes handle, mechanism, lockplate, and mounting hardware)
Neutral assembly kit - SN0610 (includes neutral assembly, bonding screw, and mounting hardware)
Cover Latch - 4056607201
Cover Latch Spring - 4022304301

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings