Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H361AWK, series F5? (may be shown as F05)
Issue:
Repair Parts

Product Line:
HD Safety Switch

Resolution:
The replacement parts for the H361AWK, series F5 (F05) are as follows. No other parts are available.
Line Base Assembly - 4056642950 (1 required; arc suppressor assembly not included)
Load Base Assembly - 4056002750 (1 required)
Arc Suppressor Assembly - 4056669451 (1 required)
Lug Assembly - CL0306F (includes 6 lugs)
Switch Mechanism - 4056610750
Handle Assembly - 4056684150K
Handle Gasket - 4056603101
Lockplate - 4056637601
Line & Load base mounting screw - 4020516001 (3 for line and 2 for load)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings