Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the DTU362AWK, series F5 (may be shown as F05)?
Issue:
Repair parts

Product Line:
Double Throw Safety Switch

Resolution:
The repair parts for the DTU362AWK, series F5 (F05) are as follows. No other parts are available.
-Line Base - 4056701350 (1 each upper and lower; arc suppressor and wire assembly not included)
-Line Base mounting screws - 4020515101 (3 required per line base)
-Arc Suppressor Assembly - 4056635550 (1 required per line base)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Wire Assembly- 4056620750 (1 required per phase; includes cable factory connected mechanical lug at one end and a crimped connector at other end)
-Line and Load Lug Assembly - CL0306F (includes 6 lugs)
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025672850 (per lug)
-Ground Lug mounting screw - 4020513503
-Switch Mechanism - 4056646950 (1 each for upper and lower)
-Linkage Assembly - 4056682750 (also replace linkage assembly rubber gaskets)
-Linkage Assembly Rubber Gaskets - 4050322801 (3 required)
-Linkage Assembly mounting screws - 2299940562 (requires 7)
-Handle - 4056688750 (handle gasket also required; lockplate gasket may also need replacing)
-Handle gasket - 4056608601
-Lockplate - 4056673301 (lockplate gasket also required)
-Lockplate gasket - 4056608601 (1 required)
-Lockplate mounting screws - 2299940562 (2 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings