Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the DTU363, series F5? (may be shown as F05)
Issue:
Repair parts

Product Line:
Double Throw Safety Switch

Resolution:
The repair parts for the DTU363, series F5 (F05) are as follows. No other parts are available.
-Line Base - 4056624750 (one each upper and lower; order arc suppressor, load lugs, and wire assembly separately)
-Line Base mounting screws - 4020515101 (3 required per line base)
-Arc Suppressor Assembly - 4056635550 (1 required per line base)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Wire Assembly- 4056780050 (1 required per phase; includes cable factory connected mechanical lug at one end and crimped connector at other end; use lug mounting screws)
-Line and Load Lug Assembly - 4025101851 (per lug)
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025101851 (per lug)
-Ground Lug mounting screw - 4020514801
-Switch Mechanism - 4056646950 (each for upper and lower)
-Linkage Assembly - 4056682750 (links together upper and lower switch mechanisms)
-Linkage Assembly mounting screws - 2299940562 (7 required)
-Handle - 4056688750
-Lockplate - 4056673301
-Lockplate mounting screws - 2299940562
-Cover Latch - 4056607201 (each for upper and lower; also requires cover latch spring)
-Cover Latch Spring - 4022304301 (each for upper and lower; also requires cover latch)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings