Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H363A, series F5? (may be shown as F05)
Issue:
Repair Parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The replacement parts for the H363A, series F5 (F05) are as follows. No other parts are available.
Interior Kit - HSIF310CF (includes line and load base assemblies, mechanism, arc suppressor, all mounting hardware, and instructions)
Load Base Kit - HLB310CF (includes load base, mounting hardware, and instructions)
Arc Suppressor Kit - HAS0610F (includes arc suppressor, mounting hardware, and instructions)
Lug Kit - CL10F (includes 6 lugs and mounting hardware)
Handle/Mechanism Kit - HM0610F (includes handle, mechanism, lockplate, gasket, all mounting hardware, and instructions)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings