Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is a WH or "water heater" breaker?
Issue:
What is a water heater QO breaker?

Product Line:
Miniature Circuit Breakers

Resolution:
It was a special QO type breaker for applications where a separate meter was supplied for a water heater. The breaker did not connect to the bus, but had two pigtails which connected to the meter, and two terminals for connection to the water heater. See pictures below:
Pic1 of water heater breaker
Pic2 of water heater breaker

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings