Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H322N, series F5? (may be shown as F05)
Issue:
Repair Parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The replacement parts for the H322N, series F5 (F05) are as follows. No other parts are available.
Line Base Assembly -4056642050 (1 required; arc suppressor assembly not included)
Load Base Assembly - 4056002550K (1 required)
Arc Suppressor Assembly - 4056001801 (1 required)
Lug Assembly - 4025101652 (per lug)
Switch Mechanism - 4056610750
Handle Assembly - 4056684150K
Lockplate - 4056637601
Neutral Assembly - SN03
Neutral Bonding Screw - 4028365650
Line & Load base mounting screws - 4020516001 (3 for line & 2 for load)
Arc suppressor mtg screw - 4020514501 (1 required)
Lockplate mtg. screw - 2299940562 (2 required)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings