Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the 9012 GNO, GPG, GQC, GRO type pressure switches available with double pole / double throw contacts?
No, this is not available in this product line. An alternative would be to use the 9012 machine tool type device digest 172 page 20-2.


CTA-ID : 11860

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings