Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What Class of fuse does the D222N, D222NRB, D322N and D322NRB general duty safety switches accept?
Issue:
Product design features

Product Line:
General Duty Safety Switches

Environment:
Fuses

Cause:
Installation

Resolution:

These switches accept Class H or K fuses as standard. For design Series F01, options include Class R fuses (field install Class R Fuse Kit RFK03H). With Class H or K fuses installed, the switch is UL listed for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current. With Class R fuses (and RFK03H fuse kit installed) the switch is UL listed for use on systems with up to 100,000 RMS Symmetrical Amperes available fault current.

NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability and will void the warranty.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings