Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
9007 Types AO12 and AW12 limit switches: what are the differences?<br />
Digest 172, pg 19-16. 9007AO12 is open type (without box) non-plug-in, with 1 NO-1 NC contacts, lever arm type; 9007AW12 is surface mounting non-plug-in standard box, with 1 NO-1 NC contacts, lever arm type. 9007AO limit switch is intended for those applications where space is at a premium so that the box is provided as part of the machine structure .


CTA-ID : 11944

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings