Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Video: Are terminal jumpers included with 9070 Type T and TF type Industrial Control Transformers?

Issue:
Terminal Jumpers may be included with some Class 9070 Type T and TF Industrial Control Transformers

Product Line:
LV Transformers

Environment:
Applies to Class 9070 Type T and TF Industrial Control Transformers by SquareD/Schneider Electric

Cause:
Some Class 9070 Type T and TF Industrial Control Transformers have primary or secondary windings that may require jumpers for interconnection to achieve various voltage levels

Resolution:
Yes.  Jumpers are shipped with 9070 Type T and TF transformers that have voltage codes that require them.

The following video demonstrates the differences between the jumpers included with 9070 series transformers:

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings