Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
9007C52B2 limit switches - Why choose the cast lever arms rather than the 360 degree angular adjustable lever arms. What`s the difference? <br />
The 360 degree has a dial-type device to set arm at various degrees around the hub of switch. In addition, there is the offset where the lever arm attaches to the switch. The effect is to allow the arm to be operated over the switch body rather than impacting. The others are flat and cannot rotate past the body.


Referred to website - Technical Library for dimensions.


CTA-ID : 12081

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings