Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an H325R, series E2, E4, and E5?

Issue:
Repair parts

Product Line:
HD Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4055218850 (3 required, arc suppressor assembly not included)
Load base assembly - 4055219050SEL (3 required)
Line and load base mounting screws - 4020600901 (2 required per base assembly)
Arc suppressor assembly - 4051204501 (3 required)
Lug assembly - 4025113650 (1 required per base assembly)
Cross arm insulators - Consists of 4 parts: (2) 4055217701 (left and right pieces), (1) 4055217801 (middle piece), and (1) 4055215701 (dust shield that ties them together behind the cross arm)
Handle assembly - 4051217251
Handle knob kit (black & red knob at end of handle) - Series E2 is 4401142750, Series E4 or E5 is 4028343550
Door thumb screw and retainer - 4405043401 & 4405043301 (Series E5 ONLY)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings