Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a H325N Series E1 and E4 Heavy Duty Safety Switch?
Issue:
Repair parts

Product Line:
Heavy Duty Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The parts listed here are the only field-replaceable parts.
Complete interior - HN325NE1 (includes line & load base assemblies, neutral assembly with bonding strap, arc suppressor assembly, Box insulator, and mounting hardware)
Line base assembly - (40552-188-50) (3-required, arc suppressor assembly not included)
Load base assembly - (40552-190-50 SEL) (3-required)
Arc suppressor assembly - 40512-045-01 (3-required)
Lug assembly - 40251-136-50 (1-required per base assembly)
Neutral assembly - (40552-252-50 SEL)
Line and load base mounting screws - 40206-009-01 (2-required per base assembly)
Handle assembly - (40512-172-50 SEL)
Handle knob kit (black & red knob at end of handle) - Series E1 is 44011-427-50, Series E4 is 40283-435-50
Door thumb screw and retainer - 44050-434-01 & 44050-490-01
Neutral bonding strap - (40283-379-50 SEL)
Cross Arm Insulator – Consists of 4 parts: (2) 40552-177-01 (left and right side pieces); (1) 40552-178-01 (centerpiece); (1) 40552-157-01 (dust shield – retainer the insulators by tying them together behind the cross arm)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings