Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an H365R, Series E2 and E4 heavy duty safety switch?
Issue:
Repair parts

Product Line:
HD Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN365E2 (includes line & load base assemblies, arc suppressor assembly, box insulator, line & load phase insulators, and mounting hardware)
Line base assembly - 4055218850 (3 required; arc suppressor assembly not included)
Load base assembly - 4055219050SEL (3 required)
Arc suppressor assembly - 4051270850SEL (3 required)
Lug assembly - 4025113650 (1 required per base assembly)
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (2 required)
Line and load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217250SEL
Handle knob kit - Series E2 is 4401142750, Series E4 is 4028343550
Door thumb screw and retainer - 4405043401 & 4405049001

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings