Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an HU265R, Series E2, E4, and E5?
Issue:
Repair parts

Product Line:
Heavy Duty Safety Switch

Resolution:

The parts listed here are the only field replaceable parts.
Complete interior - HUN265E2 (includes line base assembly, arc suppressor assembly, box insulator, line phase insulators, and mounting hardware)
Line base assembly - 4055218950SEL (2 required; arc suppressor assembly not included)
Arc suppressor assembly - 4051270850SEL (2 required)
Lug assembly - 4025113650 (1 required per base assembly)
Line base phase insulator - 4055219301 (1 required)
Line base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217250SEL
Cross Arm Insulator – (2) 4055217701 (left and right side pieces); (1) 4055217801 (center piece); (1) 4055215701 (dust shield – retainer for insulators)
Handle knob kit - Series E1 is 4401142750, Series E4 and E5 is 4028343550
Door thumb screw and retainer - 4405043401 & 4405049001

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings