Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU365R, series E2, E4, or E5 heavy duty safety switch?
Issue:
Field replaceable parts for the HU365R Series E2, E4 and E5 Heavy Duty Safety Switch

Product Line:
Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HUN365E2 (includes line base assembly, arc suppressor assembly, box insulator, line phase insulators, and mounting hardware)
Line base assembly - 4055218950SEL (3 required, arc suppressor assembly not included)
Arc suppressor assembly - 4051270850SEL (3 required)
Lug assembly - 4025113650 (1 required per base assembly)
Line base phase insulator - 4055219301 (2 required)
Line base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217250SEL
Cross Arm Insulator – (2) 4055217701 (left and right side pieces); (1) 4055217801 (center piece); (1) 4055215701 (dust shield – retainer for insulators)
Handle knob kit (black & red knob at end of handle) - 4028343550
Door thumb screw and retainer - 4405043401 & 4405049001

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings