Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there an option for Service Entrance Rating on an 8538 / 8539 combo starter?
Issue:
Do 8538 / 8539 combination starters are Service Entrance Rated?

Product Line:
Nema and Definite Purpose and Starters

Environment:
Class 8538/8539 Combination Starters

Cause:
Confirming if there's an option for Service Entrance Rating on an 8538 / 8539 combo starter.

Resolution:
No, however customer could select one of the 8940 pump panels for this application.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings