Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an HU368AWK, Series E4?
Issue:
Repair parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4401119851 (3 required; arc suppressor assembly not included)
Arc suppressor assembly - 4401139450 (3 required)
Lug assembly - 4405005402 (1 required per base assembly)
Line base phase barrier - 4401119501 (2 required)
Line base insulating plug - 4401133901
Handle assembly - 4401141351
Door thumb retainer - 4405049001
Door thumb screw - 4405043401
Handle knob kit - 4028343550
Crossbar Insulator Kit - 4051275250 (note: the metal cross bar is not replaceable)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings