Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the conductor temperature rating for the incoming lugs on main breaker and main lug HOM load centers?
Issue:
Application

Product Line:
Homeline LC

Resolution:
The lugs are suitable for 75°C conductors. 90°C conductors may be used if installed in accordance with the 2014 NEC (National Electrical Code) Article 110.14(1)(b)(2).

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings