Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU363DS, series F5 (may be shown as F05)?
Issue:
Field replaceable parts for HU363DS series F05 / F5

Product Line:
Safety Switch

Resolution:
The repair parts for the HU363DS, series F5 (F05) are as follows. No other parts are available.
-Line Base Assembly - 4056775450 (arc suppressor not included)
-Line Base mounting screw - 4020515101 (3 required)
-Arc Suppressor Assembly - HAS0610F (includes arc suppressor and mounting screw)
-Lug assembly - CL10F (includes 6 lugs)
-Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
-Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322803 (2 required)
-Lockplate mounting screw - 2194918121 (2 required)
-Ground Lug - 4025101851 (2 total required)
-Ground Lug Mounting Screw - 4020514801

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings