Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H221N, series F5? (may be shown as F05)
Issue:
Repair parts list for H221N, series F5

Product Line:
Heavy Duty Safety Switches

Resolution:
The repair parts for the H221N, series F5 (F05) are as follows. No other parts are available.
Line Base Assembly -4056642250 (1 required; arc suppressor assembly not included)
Load Base Assembly - 4056641050 (1 required)
Arc Suppressor Assembly - 4056001801 (1 required)
Lug Assembly - 4025101652 (per lug)
Switch Mechanism - 4056610750
Handle Assembly - 4056684150K
Lockplate - 4056637601
Neutral Assembly - SN03
Neutral Bonding Screw - 4028365650
Line & load base mounting screw - 4020516001 (3 required for line & 2 required for load base assemblies)
Arc suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings