Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H363NRB series F3? (may be shown as F03)
Issue:
Repair Parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the H363NRB, series F3 (F03) are as follows. No other parts are available.

Interior kit - HSIF310F (Includes line & load base assemblies, mechanism, arc suppressor, all mounting hardware and instructions)
Load base kit - HLB310F (includes load base & mounting hardware)
Arc Suppressor kit - HAS0610F - (includes arc suppressor & mounting hardware)
Lug kit - AL10F - (kit includes 6 lugs)
Handle/Mechanism kit- HM0610F (kit includes handle, mechanism, lockplate & mounting hardware)
Neutral Assembly - SN0610 (includes neutral assembly & bonding screw)
Neutral bonding screw - 40283-456-51 (Obsolete - replaced by 40283-656-50)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings