Issue:
product design features
Product Line:
EZM Metering
Resolution:
The EZM11600TB and EZM31600TB main terminal boxes will accept as standard (6) 1/0 - 600 kcmil OR (12) 1/0 - 300 kcmil Al/Cu wires per phase and neutral. The ground lug will accept (1) #6 - 300 kcmil Al/Cu wire.
product design features
Product Line:
EZM Metering
Resolution:
The EZM11600TB and EZM31600TB main terminal boxes will accept as standard (6) 1/0 - 600 kcmil OR (12) 1/0 - 300 kcmil Al/Cu wires per phase and neutral. The ground lug will accept (1) #6 - 300 kcmil Al/Cu wire.
Released for: Schneider Electric USA