Issue:
Specifications may call for copper windings on transformers
Product Line:
LV Transformers
Environment:
Are copper windings standard for the Sealed Resin Epoxy Encapsulated Transformers from SquareD/Schneider Electric?
Cause:
Some Transformer products are available with both aluminum and copper windings
Resolution:
Yes, all Square D Sealed Resin Epoxy Encapsulated Transformers have copper windings.
Square D Sealed Resin Epoxy Encapsulated Transformers are in enclosure styles A, B and C as found in the Digest.
Released for: Schneider Electric USA