Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H362, Series F2? (may be shown as F02)
Issue:
Previous Design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The repair parts for the H362, series F2 (F02) are as follows. No other parts are available.

Interior kit - HSIF3606F (includes line and load base assemblies, mechanism, arc suppressor, all mounting hardware, and instructions)
Load Base kit - HLB3606F (includes load base and mounting hardware)
Arc Suppressor kit - HAS0610F (includes arc suppressor and mounting hardware)
Lug kit - AL0306F (includes 6 lugs, mounting hardware, and instructions)
Handle/Mechanism kit - HM0610F (includes handle, mechanism, lockplate, and mounting hardware)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings