Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H362N, series F3? (may be shown as F03)
Issue:
What are the repair parts for the H362N, series F3? (may be shown as F03)

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the H362N, series F3 (F03) are as follows. No other parts are available.
Interior Kit - HSIF3606F (includes line & load base assemblies, arc suppressor, mechanism, mounting hardware, and instructions)
Load Base kit - HLB3606F (includes load base, mounting hardware, and instructions)
Arc Suppressor kit - HAS0610F (includes arc suppressor, mounting hardware, and instructions)
Lug kit - AL0306F (includes 6 lugs, mounting hardware, and instructions)
Handle/Mechanism kit - HM0610F (includes handle, handle gasket, mechanism, lockplate, mounting hardware, and instructions)
Neutral Assembly - SN0610
Neutral Bonding Screw - 4028365650
Cover Latch – 4056607201
Cover Latch Spring - 4022304301

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings