Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H362NRB, series F1 or F01?
Issue:
What are the replacement parts for the H362NRB, series F1 or F01?

Product Line:
Safety Switch​

Resolution:
The repair parts for the H362NRB, series F1 (F01) are as follows. No other parts are available.
  • Interior Kit - HSIF3606F (includes line and load base assemblies, arc suppressor, mechanism, mounting hardware, and instructions)
  • Load Base kit - HLB3606F (includes load base, mounting hardware, and instructions)
  • Arc Suppressor kit - HAS0610F (includes arc suppressor, mounting hardware, and instructions)
  • Lug kit - AL0306F (includes 6 lugs, mounting hardware, and instructions)
  • Handle/Mechanism kit - HM0610F (includes handle, handle gasket, mechanism, lockplate, mounting hardware, and instructions)
  • Neutral Assembly - SN0610
  • Neutral Bonding Screw - 4028365650

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings