Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an PAK41CTG, Series E02?
Issue:
Repair parts list for PAK41CTG

Product Line:
ServicePak Outlet Panels

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4054005101
Cover Mounting Screws - 2142717161 (2 required)
Interior Trim - 4054021401
Interior Trim Mounting Screw - 4020513001K (2 required)
Interior Assembly - 4054031250 (includes base assembly, circuit breakers, and receptacles below)
Base Assembly - 4054010650
Circuit Breaker - QO120GFI and QO130
Receptacle - 4054001450 (125 volt/20 amp) and 4054004450 (125 volt/30 amp)
Receptacle Mounting Screw - 2190312160 (2 required for the 125 volt/20 amp receptacle)
Receptacle Mounting Spring Clip - 2330100001 (2 required for the 125 volt/20 amp receptacle)
Receptacle Mounting Screw - 2159412120 (3 required for the 125 volt/30 amp receptacle)
Ground Bar - 4023089855
Ground Bar Mounting Screw - 4020547901
Closing Cap - BCAP
Closing Cap Mounting Screw - 2142720241 (2 required)
Note: Covers and Interior Trims do not have labels applied.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings