Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H322AWK, series F3? (may be shown as F03).
Issue:
Repair parts list for H322AWK, series F3

Product Line:
Safety Switches

Resolution:
The repair parts for the H322AWK, series F3 (F03) are as follows. No other parts are available.
Interior Kit - HSIF3603206CF (includes line & load base assemblies, arc suppressor, mechanism, fuse pullers, mounting hardware, and instructions)
Load Base kit - HLB3603206CF (includes load base, mounting hardware, and instructions)
Arc Suppressor kit - HAS0610F (includes arc suppressor, mounting hardware, and instructions)
Lug kit - CL0306F (includes 6 Cu. lugs, mounting hardware, and instructions)
Handle/Mechanism kit - HM0610F (includes handle, handle gasket, mechanism, lockplate, mounting hardware, and instructions)
Fuse puller kit - FPK0610

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings