Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the auxiliary/alarm contact ratings for the 9065 Motor Logic Plus Overload Relays?
Issue:
Contact rating information for 9065 overlod relays

Product Line:
Class 9065 Motor Logic solid-state overload relays (SSOLRs)

Environment:
Products sold and used in the United States

Resolution:
They are rated 10A at 120 to 240Vac or 24 to 28Vdc, with a pilot duty rating of 2000 va maximum. These contacts are not isolated.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings